Edmund Optics® (EO), the premier provider of optical components, continuously expands its product offering to reflect market developments and customer needs. On a monthly basis, new products are added to even better serve the industry. This release features details about the recent additions including TECHSPEC® Ultrafast Harmonic Separators and TECHSPEC® λ/40 Aspheric Lenses.
Edmund Optics® TECHSPEC® Ultrafast Harmonic Separators, also known as Ultrafast Harmonic Beamsplitters, reflect second or third harmonic wavelengths from femtosecond lasers and transmit the fundamental pulse. The reflective surface is designed to be highly reflective and to minimize dispersion with a GDD of ±20fs2, while the back surface is coated with an anti-reflection coating to maximize transmission. Manufactured from low wavefront distortion, 10-5 surface quality fused silica substrates, TECHPSEC® Ultrafast Harmonic Separators are available in two designs for separating harmonics of either 800nm or 1030nm lasers.
New TECHSPEC® λ/40 Aspheric Lenses feature a high numerical aperture design and an aspheric figure error of λ/40 or better, achieved via precision magnetorheological finishing (MRF). These aspheres are also available coated for specific Nd:YAG laser wavelengths as the TECHSPEC® λ/40 Laser Grade Aspheric Lenses. Each TECHSPEC® λ/40 Aspheric Lens is individually measured for 3D surface profile and test data is provided for each lens.
To view these products and the many more exciting new products offered at Edmund Optics®, visit the new products page, at edmundoptics.com.
About EO:
Edmund Optics® (EO) is a leading global supplier of optics, imaging, and photonics technology that has served a variety of markets including Life Sciences, Biomedical, Industrial Inspection, Semiconductor, R&D, and Defense since 1942. EO designs and manufactures a wide array of optical components, multi-element lenses, imaging systems, and optomechanical equipment, while supporting OEM applications with volume production of stock and custom products. With locations in more than seven countries across the globe, EO employs over 1,000 employees and continues to expand. Customers can purchase items by calling 1-800-363-1992, via the catalog or the website at www.edmundoptics.com.