eo_logo
 
Product added to cart
Anti-Reflection (AR) Coatings
Edmund Optics Inc.

Anti-Reflection (AR) Coatings

This is Section 11.3 of the Laser Optics Resource Guide.

Edmund Optics offers all TECHSPEC® transmissive optics with a variety of anti-reflection (AR) coating options that vastly improve the efficiency of the optic by increasing transmission, enhancing contrast, and eliminating ghost images. Most AR coatings are also very durable, with resistance to both physical and environmental damage. For these reasons, the vast majority of transmissive optics include some form of anti-reflection coating. When specifying an AR coating to suit your specific application, you must first be fully aware of the full spectral range of your system. While an AR coating can significantly improve the performance of an optical system, using the coating at wavelengths outside the design wavelength range could potentially decrease the performance of the system.

Why Choose an Anti-Reflection Coating?

Due to Fresnel reflection, as light passes from air through an uncoated glass substrate approximately 4% of the light will be reflected at each interface. This results in a total transmission of only 92% of the incident light, which can be extremely detrimental in many applications (Figure 1). Excess reflected light reduces throughput and can lead to laser-induced damage in laser applications. Anti-reflection (AR) coatings are applied to optical surfaces to increase the throughput of a system and reduce hazards caused by reflections that travel backwards through the system and create ghost images. Back reflections also destabilize laser systems by allowing unwanted light to enter the laser cavity. AR coatings are especially important for systems containing multiple transmitting optical elements. Many low-light systems incorporate AR coated optics to allow for efficient use of light.

Figure 1: Fresnel reflections occur at every material interface. Part of every reflected ray will experience additional Fresnel reflection each time it reaches an additional interface1
Figure 1: Fresnel reflections occur at every material interface. Part of every reflected ray will experience additional Fresnel reflection each time it reaches an additional interface1

AR coatings are designed so that the relative phase shift between the beam reflected at the upper and lower boundaries of a thin film is 180°. Destructive interference between the two reflected beams occurs, which cancels out both beams before they exit the surface (Figure 2). The optical thickness of the optical coating must be an odd integer multiple of $\tfrac{\lambda}{4}$, where $ \small{\lambda} $ is the design wavelength or wavelength being optimized for peak performance in order to achieve the desired path difference of $\tfrac{\lambda}{2}$ between the reflected beams. When achieved, this will lead to the cancellation of the beams. The index of refraction of a thin film $ \small{\left( n_f \right)} $ needed for complete cancelation of the reflected beams can be found by using the refractive indices of the incident medium $ \small{\left( n_0 \right)} $ and the substrate $ \small{\left( n_s \right)} $.

(1)$$ n_f = \sqrt {n_0 \, n_s} $$

Figure 2: The refractive index and thickness of every coating layer is carefully controlled in order to cause destructive interference between every reflected beam
Figure 2: The refractive index and thickness of every coating layer is carefully controlled in order to cause destructive interference between every reflected beam

Anti-reflection V-coats are a type of AR coating designed to increase transmission over a very narrow waveband centered at a specified design wavelength (DWL). This coating type is called “V-coat” because the curve of the transmission versus wavelength forms a “V,” with a minimum at the DWL. V-coats are ideal for obtaining maximum transmission when using single-frequency, small linewidth lasers, or narrow full width-half max (FWHM) light sources.1 V-coats typically have a reflectivity of less than 0.25% at the DWL. However, the reflection curve for the coating locally has a nearly parabolic shape and the reflectivity is significantly higher at wavelengths besides the DWL (Figure 3).

Figure 3: Example of a laser V-coat designed for maximum transmission at 266nm
Figure 3: Example of a laser V-coat designed for maximum transmission at 266nm

Table 1 shows the reflectivity and guaranteed laser-induced damage threshold (LIDT) for Edmund Optics’ standard laser V-coats.

STANDARD LASER V-COATS
DWL (nm) Coating Specifications Damage Threshold, Pulsed $ \left( \tfrac{\text{J}}{\text{cm}^2} \right) $
266 R <0.25% @ DWL 3 @ 266nm, 20ns, 20Hz
343 R <0.25% @ DWL 7.5 @ 343nm, 20ns, 20Hz
355 R <0.25% @ DWL 7.5 @ 355nm, 20ns, 20Hz
515 R <0.25% @ DWL 10 @ 515nm, 20ns, 20Hz
532 R <0.25% @ DWL 10 @ 532nm, 20ns, 20Hz
980 R <0.25% @ DWL 10 @ 980nm, 20ns, 20Hz
1030 R <0.25% @ DWL 15 @ 1030nm, 20ns, 20Hz
1064 R <0.25% @ DWL 15 @ 1064nm, 20ns, 20Hz
Table 1: Reflectivity specifications and guaranteed laser-induced damage thresholds for Edmund Optics’ standard laser V-coats – custom wavelengths available upon request

Because reflectivity increases rapidly as the wavelength of the source moves further away from the DWL, optical components with V-coats are meant for use at exactly or very close to the intended DWL of the coating. An interesting characteristic of V-coats is that the shape of their transmission curves is semi-periodic such that the reflectivity reaches a local minimum at harmonics of the DWL (e.g. $ \tfrac{\lambda_0}{2} $ or $ \tfrac{\lambda_0}{4} $) that are not as optimized for reflectivity as at the DWL. V-coats are usually comprised of only two coating layers. Simple V-coats can consist of a single layer with a thickness of a $ \tfrac{\lambda}{4} $, but more layers may be required to adjust the bandwidth or if a coating material with an appropriate index of refraction is not available. Multilayer coatings may also compensate for different angles of incidence, but are more complicated and tend to have larger bandwidths. If the thickness of the V-coat layers is incorrect, the reflectivity of the coating increases and the DWL changes. V-coats from Edmund Optics typically achieve minimum reflectivities significantly less than 0.25%, but all standard V-coats have specified reflectivities of <0.25% at the DWL. This allows for small shifts in the DWL from coating tolerances.

Broadband anti-reflection (BBAR) coatings are designed to improve transmission over a much wider waveband. They are commonly used with broad-spectrum light sources and lasers with multiple-harmonic generation. BBAR coatings typically do not achieve reflectivity values quite as low as V-coats but are more versatile because of their wider transmission band. In addition to being applied to transmissive optical components including lenses and windows, AR coatings are also used on laser crystals and nonlinear crystals to minimize reflections, as Fresnel reflections occur where air and the crystal meet.1

Broadband Anti-Reflection (BBAR) Coating Options

Edmund Optics offers all TECHSPEC® lenses with an optional single-layer, dielectric anti-reflection (AR) coating to reduce surface reflections. In addition, custom single-layer, multi-layer, V, and 2V coatings are available for both our off-the-shelf and large volume custom orders. View Custom Optical Lens Coatings for information.

Figure 4: Wavelength selection chart
Figure 4: Wavelength selection chart

$\tfrac{\lambda}{4}$ MgF2: The simplest AR coating used is $ \tfrac{\lambda}{4} $ MgF2 centered at 550nm (with an index of refraction of 1.38 at 550nm). MgF2 coating is ideal for broadband use though it gives varied results depending upon the glass type involved.

VIS 0° and VIS 45°: VIS 0° (for 0° angle of incidence) and VIS 45° (for 45° angle of incidence) provide optimized transmission for 425 – 675nm, reducing average reflection to 0.4% and 0.75% respectively. VIS 0° AR coating is preferred over MgF2 for visible applications.

VIS-NIR: Our visible/near-infrared broadband anti-reflection coating is specially optimized to yield maximum transmission (>99%) in the near-infrared.

Telecom-NIR: Our telecom/near-infrared is a specialized broadband AR coating for popular telecommunications wavelengths from 1200 – 1600nm.

UV-AR and UV-VIS: Ultraviolet coatings are applied to our UV fused silica lenses and UV fused silica windows to increase their coating performance in the ultraviolet region.

NIR I and NIR II: Our near-infrared I and near-infrared II broadband AR coatings offer exceptional performance in near-infrared wavelengths of common fiber optics, laser diode modules, and LED lights.

SWIR: Shortwave infrared broadband AR coating for applications from 900 - 1700nm.

Figure 5, Figure 6, and Table 2 show Edmund Optics’ standard BBAR coating options.


Figure 5: Edmund Optics' standard AR coatings for the visible spectrum
Figure 6: Edmund Optics' standard AR coatings for the near infrared (NIR) spectrum
Figure 6: Edmund Optics' standard AR coatings for the near-infrared (NIR) spectrum cover 400 - 1600nm, but custom coatings can be designed out past 2µm
Figure 7: Edmund Optics' standard AR coatings for the infrared (IR) spectrum
Figure 7: Edmund Optics' standard AR coatings for the infrared (IR) spectrum
Standard Broadband Anti-Reflection Coatings
Coating Description Specifications Coating Curves
λ/4 MgF2 @ 550nm Ravg ≤ 1.75% @ 400 - 700nm Download Curve
UV-AR [250-425nm] Rabs ≤ 1.0% @ 250 - 425nm< Download Curve
Ravg ≤ 0.75% @ 250 - 425nm
Ravg ≤ 0.5% @ 370 - 420nm
Laser UV-VIS [250-532nm] Rabs≤1.0% @ 250 - 532nm Download Curve
UV-VIS [250-700nm] Ravg≤0.75% @ 350 - 450nm Download Curve
Ravg≤0.5% @ 250 - 700nm
VIS-EXT [350-700nm] Ravg ≤ 0.5% @ 350 - 700nm Download Curve
VIS-EXT+ [350-700nm] Rabs <1.5% @ 350 - 700nm @ ±30° AOI Download Curve
Ravg <0.5% @ 350 - 700nm @ ±30° AOI
VIS-NIR [400-1000nm] Rabs ≤ 0.25% @ 880nm Download Curve
Ravg ≤ 1.25% @ 400 - 870nm
Ravg ≤ 1.25% @ 890 - 1000nm
Laser VIS-NIR [500-1090nm] Ravg ≤ 1.0% @ 500 - 1090nm Download Curve
VIS 0° [425-675nm] Ravg ≤ 0.4% @ 425 - 675nm Download Curve
YAG-BBAR [500-1100nm] Rabs ≤ 0.25% @ 532nm Download Curve
Rabs ≤ 0.25% @ 1064nm
Ravg ≤ 1.0% @ 1100nm
NIR I [600-1050nm] Ravg ≤ 0.5% @ 600 - 1050nm Download Curve
NIR+ [600-1050nm] Rabs <1.5% @ 600 - 1050nm @ ±30° AOI Download Curve
Ravg <0.5% @ 600 - 1050nm @ ±30° AOI/td>
NIR II [750-1550nm] Rabs ≤ 1.5% @ 750 - 800nm Download Curve
Rabs ≤ 1.0% @ 800 - 1550nm
Ravg ≤ 0.7% @ 750 - 1550nm
SWIR [900-1700nm] Ravg ≤ 1.0% @ 900 - 1700nm Download Curve
Rabs ≤ 1.5% @ 900 - 1700nm
SWIR+ [900-1700nm] Rabs <1% @ 900 - 1700nm @ ±30° AOI Download Curve
Ravg <0.5% @ 900 - 1700nm @ ±30° AOI
Laser NIR [1030-1550nm] Ravg ≤ 0.7% @ 1030 - 1550nm Download Curve
2μm BBAR [1900-2100nm] Ravg ≤ 0.5% @ 1900 - 2100nm Download Curve
Rabs ≤ 0.25% @ 1900 - 2100nm
Table 2: Reflectivity specifications for Edmund Optics' standard BBAR coatings

Anti-reflection coatings are available on the following TECHSPEC® Optics

Reference

  1. Paschotta, Rüdiger. Encyclopedia of Laser Physics and Technology, RP Photonics, October 2017, www.rp-photonics.com/encyclopedia.html

 

More Resources

Was this content useful to you?