eo_logo
 
Product added to cart
Confocal Microscopy

Confocal Microscopy

Authors: Maura Francis, Cory Boone, Jaclyn Wycoff

Confocal microscopy is a type of fluorescence microscopy which uses a laser to excite fluorescence from fluorophores used to label different subsets of a specimen. Fluorescence microscopes are used for imaging cells and tissues that have been fluorescently tagged.1 What separates confocal microscopy from conventional epi-fluorescence microscopy is its increased resolution when imaging thick specimens, elimination of out-of-focus glare due to spatial filtering, and reduction of light-induced damage to the sample, known as phototoxicity.

Instead of using an incoherent tungsten or mercury lamp source like conventional microscopes, confocal microscopes use a laser to illuminate the sample.1 The system then collects images at planes at various depths in the sample, known as optical sections, by scanning the laser through different focus positions.1 Optical sections enable live specimens to be imaged because the sample doesn’t need to be physically sectioned off. The illumination of smaller sections also helps specimens to remain viable longer by significantly reducing the effects of phototoxicity. The amount of light that conventional techniques use for illumination makes it difficult to ensure the vitality of the specimen imaged, which is crucial when capturing biological events.1

Image Appearance

When compared to images captured by a conventional fluorescence microscope, images from a confocal microscope system exhibit a marginal increase in axial and lateral resolution, but spatial filtering from the system’s pinhole assembly blocks out-of-focus fluorescence for a much more detailed image (Figure 1).2 Contrast of the image is improved over traditional methods due to a reduction in background noise and improved signal-to-noise ratio. When using conventional techniques, the fluorescence emitted from adjacent parts of the sample interferes with the image plane and obscures the focus.1 This is problematic because there is no way of differentiating the fluorescence that does not contribute to the focal plane being imaged, which is especially apparent in specimens that are thicker than two micrometers.1 By utilizing spatial filtering techniques, confocal microscopes are able to eliminate this problem by blocking any out-of-focus light that would otherwise obscure the image.2 Confocal and multiphoton microscopy have similar resolution in the x- and y-axes, but multiphoton microscopy has superior resolution in the z-axis, or depth. Compared to multiphoton microscopy, confocal microscopy only uses a single photon to excite fluorescent dyes, which can result in more light scatter in the image and the inability to image as deep into a sample. Confocal techniques commonly use light from the visible spectrum, which also tends to scatter and absorb more in biological tissue than longer wavelengths, which in turn can limit the possible penetration depth into a sample. However, the confocal technique still has proven to have enhanced resolution over traditional widefield techniques, allowing it to be considered a bridge between classic widefield methods and more advanced super-resolution techniques. Confocal microscopy is very well-suited for imaging of 2D cell cultures while multiphoton and light sheet microscopy provide advantages for imaging 3D samples.

Figure 1: An image of protoplasts captured using confocal microscopy (left) that is more finely focused than an image of microspheres of a similar size captured using conventional epi-fluorescence microscopy.
Figure 1: An image of protoplasts captured using confocal microscopy (left) that is more finely focused than an image of microspheres of a similar size captured using conventional epi-fluorescence microscopy.
Figure 1: An image of protoplasts captured using confocal microscopy (left) that is more finely focused than an image of microspheres of a similar size captured using conventional epi-fluorescence microscopy.

Technical Details

Figure 2 depicts the typical layout of a confocal microscope in which there are four key components:

  1. Laser Excitation Source: emits a laser beam into the system to focus on the sample.
  2. Fluorescence Dichroic Filters: reflects the excitation light onto the specimen and passes the secondary fluorescence, given off by the specimen, through to the detection system.
  3. Pinhole: an essential component of confocal setups, it acts as a spatial filter. It prevents any light that is not confocal to the objective focal plane from interfering with the image.2
  4. Stepper Motors: allows the laser beam to travel incrementally across the sample, obtaining x and y scans collected along the z-axis. This automates three-dimensional data being collected, making it easy to create a 3D image.2
  5. Objective: a high numerical aperture (NA) objective is typically used to achieve high resolutions. Water or oil immersion designs are often used to adjust for refractive index mismatch between the aqueous medium many live samples are kept in. Long working distances are required for thick specimens and 3D imaging/optical sectioning.
Figure 2: Schematic of a typical confocal microscopy system
Figure 2: Schematic of a typical confocal microscopy system

Comparison to Other Microscopy Techniques3

Technique Resolution Sample Size Relative Cost Photobleacing
Confocal Microscopy <µm µm $$ Yes
Multiphoton Microscopy <µm mm $$$ Less
Light Sheet Fluorescence Microscopy µm >cm $ Least


Confocal Microscopy at Edmund Optics®


Edmund Optics® supplies a wide range of optics for confocal fluorescence microscopy applications including filters, objectives, laser systems, and pinholes.

Fluorescence Filter Sets

techspec Fluorescence Filter Sets

  • Excitation, Emission, and Dichroic Filters for Fluorescence Imaging
  • >93% Transmission and OD 6 Blocking for Maximum Brightness and Contrast
  • Hard Sputtered Coatings on Single Substrate

BUY NOW

Pre-Mounted Fluorescence Filter Cube Sets

techspec Pre-Mounted Fluorescence Filter Cube Sets

  • Ensure Proper Alignment of Filter Sets
  • Easily Adapt to Common Microscopes
  • Available in a Variety of Wavelengths

BUY NOW

Fluorescence Bandpass Filters

techspec Fluorescence Bandpass Filters

  • Common Wavelengths for Popular Fluorophores
  • Excitation Filters and Emission Filters Available
  • >93% Transmission
  • >OD 6 Blocking, <3% from Edge of Bandwidth

BUY NOW

High Performance Fluorescence Dichroic Filters

techspec High Performance Fluorescence Dichroic Filters

  • Improved Flatness, Transmitted Wavefront, and Surface Quality
  • Ideal for Fluorescence Microscopy or High Magnification Imaging Applications
  • Most Popular Cut-On Wavelengths of Fluorescence and Longpass Dichroic Filters

BUY NOW

Olympus Water Immersion Objectives

Olympus Water Immersion Objectives

  • Water Immersion Objectives with Magnification Ranges from 10 to 40X
  • Displays Flat Images from High Transmission Factors up to the Near-Infrared Region of the Spectrum
  • Ideal for Fluorescence Imaging of Tissue and Specimens, such as Brain Tissue

BUY NOW

Olympus X-Line Extended Apochromat Objectives

Olympus X-Line Extended Apochromat Objectives

  • High Numerical Aperture (NA) up to 1.45
  • Chromatic Aberration Correction from 400 - 1000nm
  • Uniform Image Flatness over Large FOVs

BUY NOW

Mitutoyo Infinity Corrected Long Working Distance Objectives

Mitutoyo Infinity Corrected Long Working Distance Objectives

  • Long Working Distances
  • Bright Field Inspection
  • High Quality Plan Apochromat Design
  • Flat Image Surface over Entire Field of View

BUY NOW

Coherent High Performance OBIS LX/LS Laser Systems

Coherent® High Performance OBIS™ LX/LS Laser Systems

  • Same Compact Design for All Wavelength Options
  • Integrated Control Electronics with Analog and Digital Modulation
  • Circular Beam with Superior Beam Quality

BUY NOW

Coherent High Performance OBIS™ LX/LS Fiber-Pigtailed Laser Systems

Coherent® High Performance OBIS™ LX/LS Fiber-Pigtailed Laser Systems

  • High Performance OBIS™ LX/LS Lasers with Added Fiber Optic Capability
  • Permanent Fiber Attachment Extends Lifetime with Guaranteed Power
  • Single-Mode Polarization-Maintaining Fiber with an FC/APC Connector Provide High-Quality and Low-Noise Laser Beam Output

BUY NOW

Precision Pinholes

Precision Pinholes

  • Available in Aperture Mounts for a Secure Mechanical Support
  • Pinhole Sizes Ranging from 1 to 1,000 Microns
  • High Power Apertures Available

BUY NOW

Acktar Blackened Pinholes

Acktar Blackened Pinholes

  • Low Reflectance from the EUV to SWIR
  • 99% Absorbance Blackening Coating
  • Aperture Sizes from 20 to 1000μm
  • Available Unmounted and Mounted

BUY NOW

References

  1. Paddock, Stephen W., et al. “Introductory Confocal Concepts.” Nikon, https://www.microscopyu.com/techniques/confocal/introductory-confocal-concepts.
  2. Fellers, Thomas J., and Michael W. Davidson. “Introduction to Confocal Microscopy.” Olympus Scientific Solutions Americas Corp., https://www.olympus-lifescience.com/ru/microscope-resource/primer/techniques/confocal/confocalintro/.
  3. Santi, P. A. (2011). Light Sheet Fluorescence Microscopy. J Histochem Cytochem, 59(2), 129-138. doi: 10.1369/0022155410394857.

Additional Resources

Was this content useful to you?