The calculated distance between two exactly opposed points on a beam at a chosen fraction of peak power (typically 1/e2). It is also defined as the diameter of a circular aperture that will pass a specified percentage (usually 90%) of the total beam energy.
See also Beam Divergence , Beam Expander , Beam Width