eo_logo
 
Product added to cart

 

Utilize information from the UV and IR spectra

 

Identify weeds, pests, and crop deficiencies for agriculture

 

Analyze weather patterns, deforestation patterns, and ecosystem degradation

 

Detect and diagnose subdermal diseases including cancers early

Please accept marketing-cookies to watch this video.

Maximize Image Information with Expanded Wavebands

Hyperspectral imaging (HSI) and multispectral imaging (MSI) are two related technologies that make use of specialized vision systems to acquire extra image information from extended regions of the electromagnetic spectrum aside from the visible spectrum (Figure 1).

The visible wavelength spectrum is only a small fraction of the entire electromagnetic spectrum, and HSI and MSI utilize additional wavelengths to gather more information.
Figure 1: The visible wavelength spectrum is only a small fraction of the entire electromagnetic spectrum, and HSI and MSI utilize additional wavelengths to gather more information.

These technologies, while similar, vary slightly and are useful for their own application spaces. While these technologies provide superior image information, the systems used feature much more complexity in lighting, filter, and optical design.

Imaging Techniques

Typical machine vision systems only make use of light in the visible spectrum (from 400 to 700nm) and most machine vision sensors have peak spectral sensitives at around 550nm. Sensor sensitivity is given by the quantum efficiency curve and describes, for a particular sensor, the efficiency of converting photons of a particular wavelength into an electrical signal. However, quantum efficiencies for standard silicon sensors decrease into the UV and IR wavelengths ranges (Figure 2).

 The quantum efficiency curve for an RGB camera showing the overlap between red, green, and blue sensitivities.
Figure 2: The quantum efficiency curve for an RGB camera showing the overlap between red, green, and blue sensitivities.

HS and MS imaging techniques make use of specialized imaging lenses and machine vision sensors to collect image detail information about the object and environment a much greater portion of the electromagnetic spectrum than standard vision systems for visible light. These specialized sensors are significantly more expensive to manufacture as they are fabricated from substrate materials different than silicon. Materials such as indium arsenide (InAs), gallium arsenide (GaAs), and indium gallium arsenide (InGaAs) are used to do imaging for wavelengths up to 2600nm, whereas imaging for wavelengths in the NIR and through to MWIR make use of mercury cadmium telluride (MCT or HgCdTe), indium antimonide (InSb) focal plane arrays, indium gallium arsenide (InGaAs) focal plane arrays, microbolometers, and few others. These specialty sensors require larger pixel sizes and precise calibrations to achieve the required sensitivities and resolutions needed.1

Though manufactured from specialty materials, these sensors function nearly the same as conventional machine vision sensors with few caveats. Machine vision camera sensors construct two-dimensional images from output grayscale arrays which are generally used to do feature recognition for sorting, measuring, or locating objects. Conventional sensors are unable to differentiate between wavelengths of light without the use of optical filters or Bayer pattern (RGB) filters restricting the wavelengths of the light incident upon the pixel.2 It is the vision software that constructs the image from wavelength information on and around neighboring pixels. In HS images, pixels capture all the same information about coordinate location (within the pixel grid) and signal intensity. However, what was previously a 2D grayscale array for conventional images becomes a 3D array, or cube, with wavelength being the added dimension (Figure 2).

The difference between MS and HS imaging is whether wavelength information is represented discretely or continuously, respectively.
Figure 3: The difference between MS and HS imaging is whether wavelength information is represented discretely or continuously, respectively.

From Figure 3 above, it can be seen that wavelength information is collected for each pixel of the sensor array. The difference between MS and HS imaging is how the wavelength information is represented. MSI groups wavelength information into discrete bands and HSI is represented with a wavelength continuum. The technologies are therefore nearly identical with HS imaging having a higher wavelength resolution than MS imaging. For this reason, the two technologies present advantages over one another in different settings. HSI is best suited for applications sensitive to subtle difference in signal over a continuous spectrum. These subtle differences could be missed by an MSI system sampling larger wavebands. Selectively rejecting and capturing certain wavebands and not others is advantageous to HSI because processing fewer wavelengths means less overall processing time.

There are four main acquisition modes for obtaining wavelength information, each with a set of advantages and disadvantages. The whiskbroom method is a point scanning process that acquires spectral information for one spatial coordinate at a time and offers the highest level of spectral resolution but requires scanning the target area on both the x- and y- axes. This significantly adds to the total acquisition time.1 The pushbroom method is a line scanning method which captures and scans through a single row of pixels at a time until the full area is obtained. Systems using this method can be compact, low in weight, and have simpler operation. However, for this method, accurate exposure time is critical. Incorrect exposure times will create images with incorrect saturation for some spectral bands. The plane scanning method scans the entire 2D area and uses multiple image captures to create spectral depth. This capture method does not require translation of the sensor or system but it is critical that the object does not move during acquisition. The fourth and most recently developed acquisition method is the single shot, or snapshot, method. This method snaps a single shot and collects the entire HS data cube within a single integration period.1 This method is promising for the future of HS imaging, but is limited by lower spatial resolution and thus, requires development.1

The four acquisition modes (A) point scanning, or whiskbroom mode, (B) line scanning, or pushbroom mode, (C) plane scanning, or area scanning mode, and (D) single shot mode.
Figure 4: The four acquisition modes (A) point scanning, or whiskbroom mode, (B) line scanning, or pushbroom mode, (C) plane scanning, or area scanning mode, and (D) single shot mode.

Applications

A growing number of different application spaces utilize HSI and MSI including remote sensing and aerial imaging of the Earth’s surface with unmanned aerial vehicles (UAVs) and satellites. HSI and MSI photography can penetrate through Earth’s atmosphere and cloud cover to get an unobstructed view of the ground. This imaging is ideal to monitor population changes, observe geological activity, and study archeological sites. Additionally, HSI and MSI technology have been used to monitor and study environmental patterns about deforestation, ecosystem degradation, carbon recycling, and erratic weather systems. Researchers are able to use imaging data to create predictive models about global ecology which are helpful in combatting climate change and human impacts on nature.3

With the help of HS and MS imaging information, doctors are able to scan skin to detect cellular abnormalities including cancer non-invasively. This is due to the fact that certain wavelengths are able to penetrate deeper into skin than others. With this imaging technology, doctors no longer need to make inferences about a patient’s condition based upon their description of symptoms. Moreover, these imaging systems can automatically record and interpret spectral data, expediting diagnoses and reducing the time between diagnosis and treatment for better outcomes.4

Other industries benefiting from HS and MS imaging include agriculture, food quality and safety, and pharmaceuticals.5 Farmers are able to use spectral imaging systems attached to drones and tractors to scan large swaths of fields, analyzing the growth of crops, health of plants, the conditions of the soil, application of chemicals like pesticides, and the presence of harmful contagions or active infections. With this data, farmers can optimize the use of space and maximize production. These techniques are similarly beneficial in determining the health of natural forests, as shown in Figure 5 and Video 1.

These images are of a creek passing through a forest of trees. The leftmost image is a standard color image. The center image is created only from IR wavelengths outside of the visible spectrum. The third image is a false color image created from the wavelength information of the first two images and can be used to identify the health of the trees and the presence of any man-made objects. Image courtesy of Benjamin Margulies.
These images are of a creek passing through a forest of trees. The leftmost image is a standard color image. The center image is created only from IR wavelengths outside of the visible spectrum. The third image is a false color image created from the wavelength information of the first two images and can be used to identify the health of the trees and the presence of any man-made objects. Image courtesy of Benjamin Margulies.
These images are of a creek passing through a forest of trees. The leftmost image is a standard color image. The center image is created only from IR wavelengths outside of the visible spectrum. The third image is a false color image created from the wavelength information of the first two images and can be used to identify the health of the trees and the presence of any man-made objects. Image courtesy of Benjamin Margulies.
Figure 5: These images are of a creek passing through a forest of trees. The leftmost image is a standard color image. The center image is created only from IR wavelengths outside of the visible spectrum. The third image is a false color image created from the wavelength information of the first two images and can be used to identify the health of the trees and the presence of any man-made objects. Image courtesy of Benjamin Margulies.
A lens' focal length will shift when temperature change causes variation in refractive index and location of the lens.
Video 1: Learn more about how images in different spectra like the ones shown in Figure 5 can be combined to learn more about the health of plant populations.

Future developments in HSI and MSI include making these imaging systems much more compact, affordable, and user-friendly. Making this technology more accessible and easier to use across all industries will undoubtedly allow for its use in many more applications.

References

  1. Hyperspectral Imaging: A Review on UAV-Based Sensors, Data Processing and Applications for Agriculture and Forestry.
  2. Schelkanova, I., et al. “Early Optical Diagnosis of Pressure Ulcers.” Biophotonics for Medical Applications, 2015, pp. 347–375., doi:10.1016/b978-0-85709-662-3.00013-0.
  3. Unninayar, S., and L. Olsen. “Monitoring, Observations, and Remote Sensing – Global Dimensions.” Encyclopedia of Ecology, 2008, pp. 2425–2446., doi:10.1016/b978-008045405-4.00749-7.
  4. Schneider, Armin, and Hubertus Feußner. Biomedical Engineering in Gastrointestinal Surgery. Academic Press, 2017.
  5. Imaging in Dermatology, 2016; Chapter 16 – Hyperspectral and Multispectral Imaging in Dermatology.

FAQs

FAQ  Does Edmund Optics sell HSI or MSI systems?
Edmund Optics, does not sell HSI or MSI cameras. However, we do sell products designed for imaging outside of the visible spectrum, which are used in these systems. The TECHSPEC® C VIS-NIR Series Fixed Focal Length Lenses are designed for wavelengths from 425nm to 1000nm. TECHSPEC® The SWIR Series Fixed Focal Length Lenses are designed to be used at wavelengths between 900nm and 1700nm for InGaAs sensors
FAQ  Is HSI better that MSI or vice versa?

Neither technique is better than the other, but one type of imaging may be better suited for one application over another. HSI has better wavelength resolution but takes more time to collect data and provides more data than MSI which is only sensitive to some wavelength ranges and rejects others. Thus, MSI is typically a faster and less resource intensive process.

FAQ  What are HSI and MSI sensors made from and how does that differ from regular machine vision camera sensors?

Regular machine vision camera sensors are created from silicon whereas HSI and MSI sensor may be made from a variety of other materials, including but not limited to: indium arsenide (InAs), gallium arsenide (GaAs), indium gallium arsenide (InGaAs), indium antimonide (InSb), and mercury cadmium telluride (HgCdTe, also reduced to MCT).

FAQ  What applications use HSI and MSI?

HSI and MSI are used in agriculture, geographical surveying, pharmaceutical production, population modeling, and many medical sciences to name just a few spaces.

Technical Resources

Application Notes

Technical information and application examples including theoretical explanations, equations, graphical illustrations, and much more.

Sensors and Lenses
Read  

Sensor Performance and Limitations
Read  

Advanced Lens Selection
Read  

Videos

Informative corporate or instructional videos ranging from simple tips to application-based demonstrations of product advantages.

How an Edmund Optics Imaging Lens is Made 
Watch  

Working Distance and Focal Length Basics
Watch  

Lens Types, Resolution and Sensor Coverage 
Watch  

Webinars

Recorded webinars from Edmund Optics® experts on a wide range of optics and imaging topics.

Best Practices to Optimize & Validate Vision Systems
Watch  

Technical Calculators

Technical calculators based on commonly used and referenced equations in the Optics, Imaging and Photonics industries.

Imaging Lens Selector
Go  

Imaging System Parameter Calculator
Go  

Was this content useful to you?