Edmund Optics uses cookies to optimize and enhance the features and content on our website. Click “OK” for the full user experience, you can view additional information on the cookies we use by clicking the “Details” button. We do NOT sell your information from marketing cookies, we use it to improve ONLY YOUR experience with Edmund Optics.
Some of the data collected by this provider is for the purposes of personalization and measuring advertising effectiveness.
Some of the data collected by this provider is for the purposes of personalization and measuring advertising effectiveness.
Some of the data collected by this provider is for the purposes of personalization and measuring advertising effectiveness.
Cookies are small text files that can be used by websites to make a user's experience more efficient.
The law states that we can store cookies on your device if they are strictly necessary for the operation of this site. For all other types of cookies we need your permission.
This site uses different types of cookies. Some cookies are placed by third party services that appear on our pages.
You can at any time change or withdraw your consent from the Cookie Declaration on our website.
Learn more about who we are, how you can contact us and how we process personal data in our Privacy Policy.
Please state your consent ID and date when you contact us regarding your consent.
Most web browsers allow you to view your cookies in the browser preferences, typically within the "Privacy" or "Security" tab. Some browsers allow you to delete specific cookies or even prevent cookies from being created. While disallowing cookies in your browser may provide a higher level of privacy, it is not recommended since many websites require cookies to function properly. Alternatively, you can visit www.aboutcookies.org which provides directions on how to block or delete cookies on all major browsers.
|
Thermal lensing threatens to render some high-power ultrafast systems useless |
|
There are limitations to making gain media less sensitive to thermal effects |
|
Intracavity optics can be designed to minimize thermal lensing |
|
Recent advances in highly-dispersive mirrors help solve this issue |
The short pulse durations and high peak powers of ultrafast lasers make them ideal for a wide range of applications from materials processing, to medical lasers, to nonlinear imaging and microscopy. However, ultrafast lasers are particularly sensitive to thermal lensing, where heat causes either a gain medium or intracavity optics to deform or exhibit a refractive index gradient. This can be detrimental for ultrafast systems, even preventing them from mode-locking to produce a pulsed beam. Thankfully, advances in highly-dispersive intracavity mirrors from Edmund Optics’ partner UltraFast Innovations (UFI) enable the development of optics that experience negligible thermal effects.
Thermal lensing can occur if an active gain medium is hotter along the beam axis compared to the rest of the medium, resulting in a transverse refractive index gradient. This can misalign the laser cavity and lead to different laser mode profiles and drifts in beam pointing. Intracavity mirrors are also a critical part of ultrafast oscillators, and thermal effects can distort them as well. When focusing a beam in a laser crystal, changes in a mirror’s radius of curvature can change the focus position and even prevent the ultrafast laser from mode-locking, therefore rendering it useless. While not much can be done to change the inherent thermal properties of a gain medium, there is an opportunity for carefully choosing the right intracavity mirrors to prevent thermal lensing.
Recent developments in coating design have allowed for the development of low-loss, highly-dispersive mirrors with negligible thermal effects. This is achieved by careful manipulation of the different parameters of the optical coatings. In addition to thermal stability, the mirrors still need to provide high reflectivity and a negative group delay dispersion (GDD) to compensate for the positive GDD present in most optical media. Figure 1 shows the reflectivity and GDD of #17-070 (or UFI part number HD64), a highly-dispersive mirror with negligible thermal lensing designed for use with 1030nm ultrafast lasers. These mirrors are incredibly beneficial for high-power, solid-state lasers such as Yb:YAG, Nd:YAG, holmium, and thulium lasers.
These new highly-dispersive mirrors were tested to characterize their level of thermal lensing. An infrared camera (FLIR SC305) was used to monitor the temperature of intracavity mirrors inside a Yb:YAG thin-disk laser in continuous wave (CW) operation. A typical highly-reflective mirror with a GDD of -3,000 fs2 without the new thermal lensing-reducing technology experienced a temperature rise of >50K (Figure 2). This caused the laser mode and oscillator stability to deteriorate. However, highly-dispersive mirrors with GDDs of -1,000 fs2 and -3,000 fs2 were tested in the same setup and experienced temperature changes of 10K and 20K, respectively (Figures 3 and 4). These mirrors showed no noticeable thermally-induced effects on mode or oscillator stability, and the laser was able to function as intended.
Need a mirror at a different wavelength or GDD? Let us know what specifications you need. Edmund Optics® and UltraFast Innovations will collaborate to manufacture custom mirrors tailored for your needs
Dr. Vladimir Pervak, world-renowned expert in ultrafast coatings from UltraFast Innovations, answers several customer-inspired, frequently asked questions.
No, fiber lasers do not have a solid-state cavity where these thermal effects can occur, so again highly-dispersive mirrors without the thermally stable technology can be used. Low thermal lensing is, however, important for high-power, solid-state lasers such as Yb:YAG, Nd:YAG, holmium, and thulium lasers.
Yes, Edmund Optics offers low-thermal lensing mirrors as standard products available for immediate shipping. If you need one of these mirrors, such as UFI part number HD73 or another with different specifications, contact us to discuss a custom design.
No, creating low-thermal lensing mirrors requires careful manipulation of coating parameters and tradeoffs with other specifications. If thermal effects are important for your application, they must be addressed with optics specifically designed for those conditions.